Bosch Sensortec - Bosch has been active in the field of MEMS since 1988 and is one of the pioneers in microsystem-technology. Several hundred different types - ranging from pressure and acceleration to yaw sensors - have since then been manufactured. Bosch Sensortec, founded in early 2005, is a one hundred percent subsidiary of Robert Bosch GmbH. The company offers micro mechanical sensors, application and foundry service for consumer electronics, security systems and logistics.
- Product
Listing
- Featured
Products
- Company
Information
 | | BMA140 - Analog Acceleration Sensor The BMA140 is an analog, triaxial low-g acceleration sensor for consumer market applications, available in a super-flat land-grid array (LGA) package with a very small footprint of 3mm x 3mm and a height of merely 0.9mm. It allows measurements of static as well as dynamic accelerations. Due to its three perpendicular axes it gives the absolute orientation in a gravity field and enables free-fall detection.
More... |
 | | BMP085 - Digital Pressure Sensor The BMP085 is a high-precision, ultra-low power barometric pressure sensor for use in advanced mobile applications. With an absolute accuracy of 2.5hPa and a noise level of down to 0.03hPa (which is equivalent to an altitude change of 0.25m) the BMP085 offers superior performance
More... |
|
More about Bosch Sensortec
Bosch has been active in the field of MEMS since 1988 and is one of the pioneers in the microsystem-technology. Several hundred different types – ranging from pressure and acceleration to yaw sensors – have since then been manufactured for the automotive industry.
Bosch Sensortec, founded in early 2005, is a one hundred percent subsidiary of Robert Bosch GmbH. The company offers micro mechanical sensors, application and foundry service for consumer electronics, security systems and logistics.
Bosch Sensortec has access to the development and manufacturing competencies of the Bosch Automotive Electronics division in Reutlingen. The short distance between Bosch Sensortec and Bosch Automotive Electronics makes for flexible and close cooperation during all project phases.
This puts Bosch Sensortec in the position to not only focus on new applications, but to also quickly respond to special customer wishes. Due to its integration in the Bosch Group, Bosch Sensortec is capable of a rapid adaptation of existing sensors in new areas of application. Completely new and customized applications of micro mechanical systems are also being developed.
|
|
|