Analog Devices, Inc. - Analog Devices, Inc. (NYSE: ADI) is a world-leading semiconductor company specializing in high-performance analog, mixed-signal and digital signal processing (DSP) integrated circuits (ICs). More...
Since ADI was founded in 1965, its focus has been to solve the engineering challenges associated with signal processing in electronic equipment. ADI's products play a fundamental role in converting real-world phenomena such as temperature, motion, pressure, light and sound into electrical signals to be used in a wide array of applications ranging from industrial process control, factory automation, radar systems and CAT scanners to cellular base stations, broadband modems, wireless telephones, computers, cars and digital cameras. ADI's unique value to its customers is its ability to overcome the seemingly insurmountable barriers of speed, accuracy and cost, to solve intricate engineering challenges and to create ICs—whether they are general purpose or customized individual components—that enable portability, connectivity and multimedia. ADI designs, manufactures and markets high-performance, high-precision signal processing ICs that make pictures vibrant, voices clear, connections continuous and products portable. Less...
- Product
Training
- Product
Listing
- New
Products
- Featured
Products
- Tools
& Support
- Events
& Seminars
- Company
Information
- Other
Documents
 Digi-Key’s library of more than 500 exclusive PTM Online… On Demand® product training modules is a collection of training tools created with you – the busy design engineer – in mind. They are provided with the cooperation of participating supplier partners. From this one source, you can learn about the latest products and technologies, download datasheets, check inventory, contact our technical staff, and place an order for same-day shipment.
These modules are available in audio and non-audio formats and listed by supplier in easy-to-find alphabetical order. Simply locate the module that interests you and click on your format of choice. We hope you find these tools useful, and with new modules added continuously, we invite you to stop back often to see what’s new.
Product Training Modules Online...On Demand® is a registered trademark of Digi-Key Corporation.
 = Updated Product Training Module - PTM
 = New Product Training Module - PTM
To view modules, you will need Adobe Flash 8 software, or greater, installed on your computer. Adobe Flash Player is available FREE from Adobe.
Flash Player | Flash Player Support Center
 | | ADT7410 Digital Temperature Sensor Analog Devices' ADT7410 is a high accuracy digital temperature sensor in a narrow SOIC package. It contains a band gap temperature reference and a 13 bit ADC to monitor and digitize the temper-ature to a 0.0625°C resolution. The ADC resolution, by default, is set to 13 bits (0.0625°C). This can be changed to 16 bits (0.0078°C) by setting Bit 7 in the configuration register (Register Address 0x03).
More... |
 | | AD7190 Sigma-Delta Converter Analog Devices introduces a sigma-delta ADC (analog-to-digital converter) that features the industry's best combination of data rate and noise-free resolution. While the resolution of competing devices degrades quickly at speeds beyond 1kHz, ADI's 24-bit AD7190 sigma-delta ADC achieves greater than true 16-bit noise-free resolution up to 2.4kHz across all input voltages from 40mV to 5V. This level of performance allows designers to measure much smaller signals faster and with greater accuracy which can significantly improve system performance for precision instruments.
More... |
 | | ADXL345 Digital iMEMS® Motion Sensor Analog Devices' ADXL345 ultra-low-power digital accelerometer has an output data range that scales from 0.1Hz to 3.2kHz, unlike competing devices, which have fixed 100Hz, 400Hz, or 1kHz data rates. This allows portable system designers to better manage energy consumption by precisely allocating power for a given system function and reserving unused power for other uses. The ADXL345 measures dynamic acceleration resulting from motion or shock and with a 10,000-g shock rating is well suited for applications such as hard-disk drive protection in personal computers.
More... |
 | | ADL5502 - Integrated RMS and Envelope Crest-Factor RF Power Detection IC Now, cell phone designers can manage wireless handset power more efficiently, extend battery life and better process complex 3G and emerging 4G cell phone signals, with ADI's ADL5502, one of the industry's first dual-function RF detectors in a single package that combines an RMS detector with an envelope detector to facilitate the crest-factor measurement of complex signals.
The ADL5502 detector features a ±0.1 dB accuracy with crest factors up to 11 dB, which is five times more precise than competing devices. With the higher level of integration, cell phone users can expect up to 20 percent longer battery life.
More... |
Product Information
Circuits from the Lab ADI engineers share their lab work with you in these "Circuits from the Lab." You can combine these product pairings quickly and with confidence. |
Tools and Software
|
More about Analog Devices, Inc.
The ADI company brand is recognized throughout the electronics industry for innovative, high-performance technology and world-class engineering support. ADI's portfolio of more than 10,000 products serves the needs of more than 60,000 customers worldwide. ADI's brand, portfolio of products, breadth of customers and core competency in signal processing technology combine to form one of the strongest franchises in the entire semiconductor industry.
ADI currently has a worldwide workforce of approximately 8,600 employees, including 3,100 engineers. There are wafer fabrication facilities using high-performance analog manufacturing processes in Massachusetts, California and Ireland. Additional manufacturing facilities are located in the United States and the United Kingdom. Product test and assembly is conducted at our facilities in the Philippines. Corporate headquarters is located in Norwood, MA, USA.
|
Newsletters
ADI Newsletter eNewsletter Subscription Page
ADI & Digi-Key's IMAgination Series Healthcare Applications: Accuracy and Performance - with ADI Solutions
ADI's New High Performance Analog Components "Currents" is a quarterly publication (available online and in print) of new products. Get your first look at ADI's New High Performance Analog Components.
Solutions Bulletins Publication Series For the latest information on Analog Devices products and design solutions, delve into their Solutions Bulletins publication series. Choose just the product category you are most interested in, or take a full signal chain approach and read them all. Each issue is packed with our newest offerings, design ideas, selection guides, and info on obtaining free samples. is a quarterly publication (available online and in print) of new products. Get your first look at ADI's New High Performance Analog Components.For the latest information on Analog Devices products and design solutions, delve into their . Choose just the product category you are most interested in, or take a full signal chain approach and read them all. Each issue is packed with our newest offerings, design ideas, selection guides, and info on obtaining free samples. |
Product Information
 | | NAppkin Notes Written expressly for the Digital Isolation Update – are ideas, hints, and tips for building with iCoupler technology.
NAppkin Note: Isolating USB with SPI By: Mark Cantrell, Applications Engineer |
|
|